2025-01-28 1:57 AM
I have STEVAL-CTM012V1 evaluation board for 250 W. I have followed all the procedure which are mention in the manual where I first load the firmware file stsw-ctm11 in motor control work bench then click on generate code then goes into cubemx then generate code and goes into STM32CubeIDE and project is created. So my question is that the generated project is enough to run motor means we just need to upload the code into the board and it will start motor right?
2025-03-04 12:58 AM - edited 2025-03-04 1:00 AM
Hello @Aditya_sp,
For provided example usage, refer to um2963 documentation, "4 Firmware debug " chapter.
You can use X-CUBE-MCSDK-6 tool available here to generate your project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.