2025-02-28 10:01 AM
How can I change the rev-up and stop ramps programatically ?
I can change the rev-up ramp through motor pilot but I have to do it everytime it connects.
I want to control that through the program.
I'm using code generated from the MC WB / MC MX / MX IDE chain.
Board is a B-G431B-ESC1
Thank you
2025-03-03 1:01 AM
Hello @pjrebordao,
RevUp Start-up profile settings are available through MC Work bench tool>"Speed Sensing Config">"Sensorless start-up parameters" tab.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.