2025-04-04 4:29 AM - edited 2025-04-04 4:29 AM
Hello,
I was reading the RCM Regular Conversion Manager. It states that it is forbidden to add new injected channel on ADCs using current sensing. However, they do give an option to use regular conversion.
But in my case, I need to read a sensor at the same time of the current sensing. Since we have two ADCs used for current sensing since I am using STEVAL-PTOOL4A, is it possible to add this channel as injected one on both ADCs ? and what is the issue in adding it to one of the ADC as injected channel? I don't get what could be the issue?
Thank you.
Solved! Go to Solution.
2025-04-08 7:54 AM
Hello @AnthonyK,
For ADC3, if you are using a different sampling time, you are right.
Using STM32CubeMx and STEVAL-PTOOL4A schematic, you can try to find a solution that does not impact the board.
2025-04-04 7:28 AM
Hello @AnthonyK,
If you are not using High Sensitivity Observer, ADC3 is not used and PB1 Pin input is available.
2025-04-04 7:32 AM - edited 2025-04-04 8:16 AM
Aha ok, but the issue I need this additional ADC to be triggered with the same event of the current ADCs (so it is the middle of the PWM signal). Is it ok than to have an interrupt from the ADC3?
Plus if I have well understood, in the generated cubeMX from the MC Workbench, the ADC1 and ADC2 interrupts are configured as end of single conversion. However, in the generated code (in the R3_2_Init) we disable the EOC and we enable the end of sequence conversion of one of the ADCs?
2025-04-04 8:33 AM
Hello @AnthonyK,
Setting ADC3 External Trigger parameters as for ADC1 and ADC2, ADC3 Inj value will be available at the same time as the reading of the ADC1/2 current values.
2025-04-07 2:36 AM - edited 2025-04-07 2:53 AM
Thank you. But this depends also on the sample time of the ADC3. But in general, is it better to poll the EOC or to generate an interrupt which will be lower in priority than the ADC of the current? Plus, since the PB1 input uses the BEMF, I should configure the board and connect the new signal?
2025-04-08 7:54 AM
Hello @AnthonyK,
For ADC3, if you are using a different sampling time, you are right.
Using STM32CubeMx and STEVAL-PTOOL4A schematic, you can try to find a solution that does not impact the board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.