2025-04-03 1:04 AM - edited 2025-04-03 2:10 AM
Hello,
I am trying to use PC15 as GPIO input on the STEVAL-PTOOL4A. I configured it using CubeMX with pull-down resistor however the pin status is not changing in the software. I am sure my switch works well (checked on oscilloscope) and the LSE is disabled. Just I generated the code using MC Workbench and configured the PC15 as input mode. Normally it should be configured for DIR signal as per the datasheet. In addition, I have found that the J13-5 (which normally should be connected to PC15) is always at 3.3V
Is there any additional configuration that should be made?
Thank you for your support
Solved! Go to Solution.
2025-04-03 5:03 AM
It was my fault, the trigger should be connected to 0V and not 3.3V
2025-04-03 5:03 AM
It was my fault, the trigger should be connected to 0V and not 3.3V
2025-04-04 2:36 AM
Hello @AnthonyK,
Thank you for your feedback.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.