STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! EVSPIN32G06Q2S1 board damaged during power-up

Hi,We were attempting to control a high-voltage BLDC motor using the EVSPIN32G06Q2S1 evaluation board. While following the Getting Started procedure described in UM3394, the board got  damaged during the power-up stage.Below are the steps we followed...

d155ee50-4e84-4ad1-921e-96e2a7d6f9e0.png
sujay-s by Associate II
  • 737 Views
  • 6 replies
  • 2 kudos

FOC motor control with HSO and Hall sensors

Hi,I've been experimenting with the High Sensitive Observer using the B-G473E-ZEST1S and STEVAL-LVLP01 boards to control a BLDC motor. So far we have good results, however sometimes the HSO loses control, especially at very low speeds (<10 electrical...

How to apply for the Zest algorithm

Hello,I purchased the Zest development board kit. I have personally tried HSO and found it quite good. I heard that the Zest algorithm can achieve full torque output at zero speed. I am very interested in this. Could I apply for it personally?

lvtao by Associate
  • 162 Views
  • 1 replies
  • 1 kudos

Resolved! [STSPIN32G4] Radiated Emission Issue

Hello I want support for STSPIN32G4 EMI Issue I took tests for Farfield EMI Report at STSPIN32G4 Standby conditionReport shows QP are over than Limit at 190.547MHz, 253.803MHz and I also get similar result by using Near-field prove(Proved Noise Peak...

DKim39_1-1715824394066.png DKim39_2-1715824446125.png DKim39_3-1715824593906.png
DKim.39 by Associate
  • 1970 Views
  • 3 replies
  • 0 kudos

Resolved! Motor pilot connection issue

Hi Team,I am working on a custom board with STSPIN32F0601S3, after generating code using MCSDK Version 6.3.0 with cube Mx 6.10.0, I tried to connect Motor pilot just start/stop and change RPM but it did not connect, Pls confirm which steps I am missi...

Nidhi12 by Associate II
  • 779 Views
  • 6 replies
  • 0 kudos

Why No FreeRTOS available with H563ZI in MC workbench

In MCSDK 6.2.0, it says "Selected hardware boards do not support this feature". In MCSDK 6.3.2, nothing.Why?Without this, it generates MC code using systick, and if adding FreeRTOS with CubeMX, I have to merge the systick handlers for FreeRTOS and MC...

PQ by Associate II
  • 1021 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.