STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! B-G431-ESC1 Hall sensors connection issue

Hello, I am using a B-G431-ESC1 board to power some BLDC motors. I have alrady used it succesfully to spin some 2 pole pairs BLDC using Hall sensors for speed control. I even managed to implement some code to stop the motor at every half rotation of ...

Da3 by Associate II
  • 365 Views
  • 1 replies
  • 0 kudos

STSPING4 VDS protection triggered.

About EVSTSPIN32G4, I started the code generated by MotorControl Workbench 5. Y.3 normally.If you transplant the IIC configuration of the pre drive and enable PWM output, the VDS will report an error.After carefully reading the generated code, it is ...

GWenJ.1 by Associate II
  • 2065 Views
  • 8 replies
  • 1 kudos

MC Workbench - ACD1/2 porting to ADC12, STM32G474R

EDIT: Resolved! It looks like this was an issue with the pin reporting on our end.  Hello, We would like to use MC workbench, however we want to move from ADC1/2  to ADC12 for the current sense, VBUS and temperature NTC.  Is there a way to implement ...

Hattie by Associate
  • 201 Views
  • 1 replies
  • 0 kudos

STM32 MCUs Motor control WB APP failure error

I have this Fatal Error. Plese help me"  [Fatal Error] 2.STM32CUBEMX.5.6.0.AnalyticsServer.xml:1:1: Premature end of file. [Fatal Error] 2.STM32CUBEMX.AnalyticsServer.xml:1:1: Premature end of file. [Fatal Error] 2. AnalyticsServer.xml:1:1: Premature...

Screenshot 2026-05-03 115625.jpg
DODOAN by Associate
  • 213 Views
  • 1 replies
  • 0 kudos

Resolved! HSO on G431

Hi,I'm trying to setup HSO on the G431, I used the B-G431B-ESC1 board as a starting guide. I'm trying to use differential sensing with internal OP-AMPs and internal PGA. I have split the currents and phase voltages across ADC1 and ADC2 but I still ca...

sst1010 by Associate
  • 310 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.