STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! How to brake a brushless DC motor?

Hello! I'm trying to smoothly brake a three phase brushless motor, by short circuiting the phases. At this moment an overvoltage occurs damaging the power circuit. Is this the right way to do it? Thanks

Resolved! About TB6600hg stepper driver.

HI, i am using TB6600HG stepper IC in my board to drive stepper motor using stm32f103R8Tx. In TB6600hg driver IC there is a Alert Pin its function is to monitor TSD and ISD.where TSD is built in thermal shutdown.ISD is built in overcurrent detecti...

Lchal.1 by Associate III
  • 1813 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 spi receive procedure without hal

Good afternoon,I am a newbie in the programing of stm32. Just working on a project, where is a serious problem with timing. Trying to implement FOC on the PMSM motor where I need to do a calculation in 50us loop, which is fast to communicate with ang...

JSovi.1 by Associate
  • 2778 Views
  • 1 replies
  • 0 kudos

STM32H7 motor control support?

Anyone know when/if the H7 series will have more motor control support? The F series can't do what I need and only 1 chip (which has an eval board) can be used in MCWB but it is extremely limited.

GBuke.1 by Associate
  • 3606 Views
  • 6 replies
  • 1 kudos

Resolved! NEW X-CUBE-MCSDK version 5.4.5 available

Dear Motor Control customers and #[STM32 Motor Control]​ community members,We are very glad to announce the new X-Cube Motor Control SDK 5.4.5.This version is fully compatible with new CubeMX 6.1 and is still available at: https://www.st.com/en/embed...

Why is the MCSDK not using floating point algorithms?

Since I'm still fairly new to the STM / Arm world, I wonder why, for example, the X-CUBE MCSDK does NOT use the floating point algorithm for devices that have a hardware floating point unit. Are there special things to watch out for when using floati...

ben5en by Associate II
  • 1376 Views
  • 2 replies
  • 1 kudos

Why does VBUS voltage always show 0V (Under Voltage Fault) in Monitor section of ST Motor Control workbench?

I have developed a custom board using STSPIN32F0A for bldc motor control application. When I am trying to test with Bull Running BR2804 motor, after configuration of pins when I check in Monitor Section, VBUS voltage is 0 Volt and a continuous Underv...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.