STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

how does the divider work in PID tuning?

I am using NUCLEO-F303RE, X-NUCLEO-IHM08M1, MotorControl Workbench 5.4.4 and STM32CubeMX 5.5.0. I have managed to generate a project as position control and it seems to work fine however I am wondering if I can improve further the performance of the ...

msingh by Senior
  • 1578 Views
  • 2 replies
  • 1 kudos

Resolved! evspin32f0601s1 (6-step control in workbench)

I bought the evspin32f0601s1 board.In the data sheet"Sensored or sensorless 6-step algorithm"It is described like this...Is it not possible to select 6-step in the st motor control workbench?And since there is no detailed information about the workbe...

DLee.10 by Associate
  • 1220 Views
  • 1 replies
  • 1 kudos

Resolved! [CRITICAL HW BUG + FIX] STEVAL SPIN3204 board: maximum motor current not reaching 16A as claimed

PCB layout of STEVAL STSPIN3204 board contais critical bug as explained in attached report which prevents the design to work up to claimed 16Arms. This bug creates extreme radiated emissions (affecting nearby instruments) and prevents the proper func...

Pin state of STM32G431KBT in DFU boot mode

I build a custom board with the STM32G431KBT controller that drives a DC motor via a TI motor driver.When I put the board in boot mode it drives the motor at full speed.This only can happen when a combination of 4 pins is in a specific state.One PWM...

0693W000006HucTQAS.jpg
WSpar.1 by Associate III
  • 3235 Views
  • 4 replies
  • 0 kudos

IHM08M1 with NUCLEO-H743ZI2 board in FOC mode.

Hi! I need to control a BLDC motor in FOC mode. I have a NUCLEO-H743ZI and IHM08M1, I know that they are not compatible with the ST morpho connector. But I decided to connect them manually with wires.On IHM08M1 board I removed capacitors C3, C5, C7, ...

VKost.2 by Associate II
  • 1593 Views
  • 2 replies
  • 0 kudos

5V output with 3.3V input

Hi! I'm trying to control four 8520 motors with a NUCLEOf303k8. I would use two L293B for this scope, but the input voltage for my NUCLEO is 3.3V. The L293B needs an input voltage of 4,5V, at minimum. Will the NUCLEO "5V" output pin provide 5V to the...

MRoss.21 by Associate II
  • 3164 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.