2020-05-07 9:16 AM
Anyone know when/if the H7 series will have more motor control support? The F series can't do what I need and only 1 chip (which has an eval board) can be used in MCWB but it is extremely limited.
2020-05-11 12:24 AM
Dear GBuke,
We have right now, some code example for the H7 linked to the MCSDK (but as it is code example, you cannot modify it with MC workbench).
Is that helping you or do you need full H7 support?
Thanks and best regards,
Claire
2020-08-06 7:17 AM
Hi Claire,
The example given for the H7 is only for the the dual-core uC H745ZI. Any idea of when is the H7 single core going to be supported?
Thanks,
E
2020-10-14 11:46 AM
Dear @kswarm , dear @GBuke.1
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-10-15 1:31 AM
Hi Laurent, @Laurent Ca...
as you can see I never got answered the question I did, it would be nice if you could give us more information about it.
Thanks a lot!
E
2020-10-15 1:42 AM
Dear @kswarm (Community Member),
We have no plan to add STM32H7 single core in our MCSDK, sorry...
I guess the easiest solution for you will be to use an STM32F7 project and modify it.
Thanks and best regards,
Claire
2021-02-03 8:50 AM
Do plan to support any of H7? If yes, when?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.