2021-02-02 2:02 PM
Good afternoon,
I am a newbie in the programing of stm32. Just working on a project, where is a serious problem with timing. Trying to implement FOC on the PMSM motor where I need to do a calculation in 50us loop, which is fast to communicate with angle sensor via SPI and HAL. Let me explain the situation.
I tried to work with HAL, but as I read everywhere and explored by myself: if you need speed put it away. So my plan is to use CubeMX to configure all necessary registers and read data directly from the register DR. One small thing, that sensor communicates with a 16-bit frame.
Code that I produced:
__HAL_SPI_ENABLE(&hspi3);
HAL_GPIO_WritePin_Fast(GPIOD, GPIO_PIN_2, GPIO_PIN_RESET); //switch off the pin
hspi3.Instance->DR = 0;
while ((hspi3.Instance->SR & SPI_FLAG_RXNE) == 0){} //Wait for Data Ready to Read
RxByte[0] = hspi3.Instance->DR; //Read Data Register Directly
HAL_GPIO_WritePin_Fast(GPIOD, GPIO_PIN_2, GPIO_PIN_SET); // switch on the pin
__HAL_SPI_DISABLE(&hspi3);/**
* @brief SPI3 Initialization Function
* @param None
* @retval None
*/
static void MX_SPI3_Init(void)
{
/* USER CODE BEGIN SPI3_Init 0 */
/* USER CODE END SPI3_Init 0 */
/* USER CODE BEGIN SPI3_Init 1 */
/* USER CODE END SPI3_Init 1 */
/* SPI3 parameter configuration*/
hspi3.Instance = SPI3;
hspi3.Init.Mode = SPI_MODE_MASTER;
hspi3.Init.Direction = SPI_DIRECTION_2LINES;
hspi3.Init.DataSize = SPI_DATASIZE_16BIT;
hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi3.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi3.Init.NSS = SPI_NSS_SOFT;
hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi3.Init.CRCPolynomial = 7;
hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi3.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI3_Init 2 */
/* USER CODE END SPI3_Init 2 */
}In this state, it isn't working, has anyone idea how to solve this issue? Thank you
edit: already solved...
It needed to put something to DR register to init clock, which causes start the communication.
hspi3.Instance->DR = 0;
Then you need to test if data are ready for reading and then read data from register DR.
while ((hspi3.Instance->SR & SPI_FLAG_RXNE) == 0){} //Wait for Data Ready to Read
RxByte[0] = hspi3.Instance->DR; //Read Data Register Directly
Solved! Go to Solution.
2021-02-04 7:50 AM
Hello @JSovi.1 and welcome to the STM32 Community =)
I'm glad to know that you have solved your issue.
You can add a post detailing how you solved your problem ("Need to put something to DR register to init clock"). then mark it as best by clicking on the "Select as Best" button. This will help other users find this solution more quickly.
Imen
2021-02-04 7:50 AM
Hello @JSovi.1 and welcome to the STM32 Community =)
I'm glad to know that you have solved your issue.
You can add a post detailing how you solved your problem ("Need to put something to DR register to init clock"). then mark it as best by clicking on the "Select as Best" button. This will help other users find this solution more quickly.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.