2021-02-05 8:32 PM
HI, i am using TB6600HG stepper IC in my board to drive stepper motor using stm32f103R8Tx. In TB6600hg driver IC there is a Alert Pin its function is to monitor TSD and ISD.
where TSD is built in thermal shutdown.
ISD is built in overcurrent detection.
if my TSD = Under TSD detection and ISD=normal then ALERT = low.
if my TSD= normal and ISD= normal then my ALERT = z.
And even they are used 'z' for some other pins to check the state.
But I don't know what that 'z' refers or meaning in TB6600HG driver IC . can anyone help me with it please.
Thank you
Solved! Go to Solution.
2021-02-06 1:26 AM
Hello
High Z state is the third state of a Three State logic. (Hi Lo high-Z)
Z is the impendance generaly, so High Z state is like the pin is disconnected.
Formaly, a resistor is connected between this pin and Vcc (pullup).
The purpose of this logic is to use multiple devices in a single bus.
"Open Drain" used in STM32 devices is a hi-Z state.
2021-02-06 1:26 AM
Hello
High Z state is the third state of a Three State logic. (Hi Lo high-Z)
Z is the impendance generaly, so High Z state is like the pin is disconnected.
Formaly, a resistor is connected between this pin and Vcc (pullup).
The purpose of this logic is to use multiple devices in a single bus.
"Open Drain" used in STM32 devices is a hi-Z state.
2021-02-10 1:20 AM
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.