2021-05-15 5:19 PM
The function PI_Controller() implements PI control but there seems to be an error in the final output with the wDischarge term. This term is calculated at the very output as the anticipated amount the output exceeds the output limit's. The intent is to reduce the integrator by this amount but the code does not account for the Ki divisor, pHandle->hKiDivisorPOW2. Without this the value applied to the integrator is too small.
2021-05-28 5:49 AM
Dear @BTrem.1
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, and so on)?
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.