STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Cannot enter HRTIM1_Master_IRQHandler

Hello, I'm using STM32F334C8T6 and trying to measure the duration of my calculation sectionfrom MCMP1R (JEXT9) which triggers ADC1 till all TIMER's D CMP registers change.1) I enabled Global Master Timer Interrupt and MCMP1 interruptNVIC_EnableIRQ(H...

AZaya.1 by Associate
  • 1685 Views
  • 1 replies
  • 0 kudos

STM32 complimentary PWM dead-time insertion

Hello all, Currently I'm working with BLDC motor 6 step drive. I'm using complementary PWM channels. Logic works good and working with well with the hardware. But when ever i insert dead time its reducing on time of the Low side pulse (CHxN) but for ...

STM32G474 Hall sensor

Hello, I have a question regarding the use of the timer function xor input for the hall sensor in the BLDC motor, how do I read the first rotor position to start, then I understand that each timer interrupt changes the commutation.

kulfi27 by Associate II
  • 1373 Views
  • 1 replies
  • 0 kudos

I'd like to porting software from P-NUCLEO-IHM03

I'd like to porting software from P-NUCLEO-IHM03 (NUCLEO-G431RB + X-NUCLEO-IHM16M1) to NUCLEO-G474RE+ X-NUCLEO-IHM16M1.Are there hardware differences between NUCLEO-G431RB and NUCLEO-G474RE that exclude such software porting?I installed on my PC soft...

POlcz by Associate III
  • 1577 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.