2021-05-21 12:17 AM
Project details:
Control Board Nucleo-F746ZG, Power Board X-Nucleo-IHM08M1, X-CUBE-MCSDK-FUL_5. Y. 1, st-stm32cubeide_1.6.1, stm32cubemx-win_v6-2-1, stm32cubef7_v1-16-1.
Errors:
1) unknown type name 'RTC_HandleTypeDef'(if LL)...
2) RTC_HandleTypeDef hRTC_Handle; (if HAL)...
2021-05-31 4:44 AM
Dear @�?лек�?андр Микрюков
Welcome to the STM32 Community
Where are coming from the source code you are trying to build?
Best regards
Laurent Ca...
2021-05-31 10:38 PM
Good day.
The problem was solved by reinstalling Windows 10 x64 ...
But there was a new one: in the new Windows, the program Motor Pilot 5.Y.1 does not start... I tried with different versions of Microsoft Visual C++...
What could be the problem?
Sincerely, Alexander
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.