STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

STSPIN32F0 low inductance bldc motor tuning

Posted on July 31, 2017 at 12:47I am using STSPIN32F0, wich has a maximum of 12kHz FOC freq. I am trying to drive a novoMotec motor, with the attached properties. Since the FOC FAQ states that 'In the case of either a high-speed or low-inductance mo...

FOC duration fault

Posted on October 12, 2017 at 21:54Hi,Running the configuration below:-NUCLEO-F302R8-X-NUCLEO-IHM07M1-FOC SDK 4.3Succesfully tuned BLDC motor with the Motor Profiler. Also in Play Mode the motor runs very well.Next step is running the BLDC motor usi...

paul2 by Senior
  • 1259 Views
  • 1 replies
  • 0 kudos

Modify the startup PWM sequence

Posted on February 06, 2018 at 16:23I downloaded the  ST Motor Control Workbench v4.3 software to configure motor and application for FOC control 1 or 3 shunts.I use IAR Embedded Workbench (free limited version is enough) because there is already a ...

SLLIMM-1 Open failed

Posted on February 22, 2018 at 14:23I am not able to open the STEVAL-IHM040V1 FOC SDK workbench settings from st website.http://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-ihm040v1set.html I extracted the zi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.