STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

STM32 FOC SDK & CubeMX

Posted on March 15, 2016 at 15:44hi! Can be STM32 FOC SDK & CubeMX generated code used in same project? We already have some libraries based on CubeMX. 

vromanov by Associate II
  • 1558 Views
  • 2 replies
  • 0 kudos

Problem to build example with iar 7.4

Posted on March 24, 2016 at 18:42Hi, i have some problems to build a project for P-Nucleo IHM001_singledrive kit !When i open the project it said me that some options are broken and when i build the project (after use workbench tool to configure the...

idealsim by Associate II
  • 2005 Views
  • 3 replies
  • 0 kudos

Issue with FOC sdk 4.2 and stm3210B eval kit

Posted on March 25, 2016 at 16:04Hi i'm trying to work with our STM3210B eval kit (shinano MB459) but i have some problem to use it. When i launch ST Motor Control Workbench : - Choose example project STM3210B-Eval-MB459-Shinano - Check the values o...

idealsim by Associate II
  • 1391 Views
  • 2 replies
  • 0 kudos

Problems with ICS and Hall Sensors on FOC SDK 4.1

Posted on March 29, 2016 at 11:00Hi, we are using FOC SDK 4.1 with ICS current sensing and State Observer + PLL. A Motor with 21 pole pairs and Rs 11mOhms and Ls 0,017mH runs up to 6000 rpm very well.  Now changing to Speed / Feedback with Hall Sens...

UL Approval

Posted on March 30, 2016 at 18:56Hi All, We have been using FOC sdk for developing our products for a few months. Our customers are in US and they need our product approved by UL. One of our US agents told me that ''UL has been working with the BL...

KF Lam by Associate II
  • 2003 Views
  • 3 replies
  • 0 kudos

Motor Control PMSM FOC user projects location

Posted on April 11, 2016 at 23:47Hi ,I am unable to locate the user projects after installing the Motor Control SDK. Can any one tell me where I can find the user projects that interact with the FOC library - specifically I need the Keil uVision one...

imtiaz by Associate II
  • 1566 Views
  • 3 replies
  • 0 kudos

Evaluating Motor Control using AC6 Workbench for STM32

Posted on April 20, 2016 at 19:52Hello, I am trying to evaluate motor control firmware with AC6 Workbench. I am looking at the STM32 PMSM FOC SDK 4.2, Hands-on workshop with hardware tools, Rev 1.5, and it only supports Keil and IAR. Is there a vers...

jorge2 by Associate II
  • 999 Views
  • 2 replies
  • 0 kudos

Getting source files for PWM interface

Posted on April 20, 2016 at 21:40Hi,I am building my own motor control libraries, and I need an example of the PWM interface. Looking at the FOC SDK, this function, and others like this one, is of interest to me:uint16_t PWMC_SetPhaseVoltage(CPWMC t...

jorge2 by Associate II
  • 1786 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.