2016-04-20 12:40 PM
Hi,
I am building my own motor control libraries, and I need an example of the PWM interface. Looking at the FOC SDK, this function, and others like this one, is of interest to me:uint16_t PWMC_SetPhaseVoltage(CPWMC this, Volt_Components Valfa_beta);How can I get the source files for this function? It seems to be embedded in a library, but this shouldn't have any IP, since it is just a peripheral interface. Thanks for the help!2016-04-20 11:32 PM
Ciao
You have to ask the source code to your nearest ST distributor. Ciao Gigi2016-04-21 7:50 AM
Thanks, how can I find my nearest distributor? Do you have an email or phone number?
2016-04-21 8:37 AM
Never mind, I see the map on st.com, so I will give them a call.
2021-06-15 7:16 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.