2016-03-15 7:44 AM
hi!
Can be STM32 FOC SDK & CubeMX generated code used in same project? We already have some libraries based on CubeMX.2016-04-01 6:13 AM
Ciao Vladimir
No, is not possible at the moment because the FOC SDK is based on the standard peripheral library and the code generated by the CubeMX is based on CubeHAL. We plan to converge the FOC SDK versus the CubeMX but this will not be ready very soon. Ciao Gigi2021-06-17 12:58 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.