2016-03-25 8:04 AM
Hi i'm trying to work with our STM3210B eval kit (shinano MB459) but i have some problem to use it. When i launch ST Motor Control Workbench :
- Choose example project STM3210B-Eval-MB459-Shinano - Check the values of motor, micro (stm32F103 Medium) - Check pin assignment (usart1 TX A9 / RX A10) - check lcd and Serial in drive management / user Interface Add-on - choose the output folder (C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Web\SystemDriveParams) - generate the code - launch the project with Iar (C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Web\Project\EWARM\STM32F10x_Workspace) - configure Iar to build STM3210B-EVAL - project build ok - load the app in the card --> ok - reset the cardThe problem is that nothing appear on the lcd screen and serial com with ST Motor Control Workbench not work !Do you have an idea of the problem please ?edit
:Problem resolve, need to configure the use of LCD with light option (not full).Now is working2016-04-01 5:43 AM
Ciao
I give to you one more hints. The full version of the LCD needs to be programmed in a separate way respect the motor control part. All of this is explained in the UM so if you want to enjoy the full LCD you can take a look. If you didn't program the LCD and you enable it the firmware will stop and LCD and serial communication is stopped. Another option if you don't want to program the FULL LCD code is to disable it in the WB and use only the serial communication. Ciao Gigi2021-06-17 12:47 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.