2016-03-24 10:42 AM
Hi, i have some problems to build a project for P-Nucleo IHM001_singledrive kit !
When i open the project it said me that some options are broken and when i build the project (after use workbench tool to configure the motor) i have this error :startup_stm32f302.s Error[438]: This instruction is not available in the selected cpu/core C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Common\Libraries\CMSIS\CMSIS_2_x\Device\ST\STM32F30x\Source\Templates\iar\startup_stm32f302.s 173Error while running Assembler
arm_biquad_cascade_df2T_f32.c
Fatal Error[Pe1696]: cannot open source file ''arm_math.h'' C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Common\Libraries\CMSIS\CMSIS_2_x\DSP_Lib\Source\FilteringFunctions\arm_biquad_cascade_df2T_f32.c 41 Can you help please ?2016-03-29 8:59 AM
2016-04-01 5:33 AM
Ciao
Sorry for the delay... yes, updating the IAR solves the issue. Ciao Gigi2021-06-17 12:49 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.