STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Is this a 120 or 60 deg displacement angle hall motor?

Hello forum! I am trying to characterize a motor for experimentation with the workbench. I spun the rotor with a hand drill and got the following waveform, with the first 3 channels being H1, H2, H3 and the analog voltage being the back-EMF from th...

0693W000003QjGhQAK.png 0693W000003QjGrQAK.jpg
hmc by Associate III
  • 9087 Views
  • 8 replies
  • 1 kudos

Resolved! BLDC motor: How to archive higher startup torque?

Hi ST CommunityI am working on a project where I want to use a BLDC motor for a screwdriving process. The setup is based on the B-G431B-ESC1 and a Maxon motor https://www.maxongroup.com/maxon/view/product/651618 (with a 6:1 gear added). The motor con...

JA.1 by Associate III
  • 5091 Views
  • 5 replies
  • 0 kudos

Resolved! Is there a way to fine-tune motor parameters (final ramp value, speed ramp up...) in the motor workbench without systematically re-generating code from Motor Control Workbench

Hi !Is there a way to fine-tune motor parameters (final ramp value, speed ramp up...) in the motor workbench without systematically re-generting code from Motor Control Workbench and then Cube-MX everytime every time I'd like to adjust a parameter ?I...

Luczia by Associate II
  • 2268 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.