STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Resolved! The protocol of Motor control example.

When we're using Motor Control Workbench to control the motor, we can get the motor information and control the motor through Motor Control Workbench. Is this information available via UART?We need to know how Motor Control Workbench communicates wit...

Resolved! STEVAL-ESC001V1 - Workbench example doesn't work

Hi! I am trying to control sensorless BLDC motor using STEVAL-ESC001V1.I finished profiling my motor and working on the example on Workbench(STEVAL-ESC001V1 electronic speed control 5.4.0).I opened the example on the workbench and set the motor param...

Slee.3 by Associate II
  • 2338 Views
  • 5 replies
  • 0 kudos

Resolved! Output phase current being limited to 200A

Hi folksWe have a 3-shunt sensor-less FOC solution for running a PMSM motor generated from STM32 Motor Control Workbench (ver 5.4.4). The max readable current is upwards of 500A. However, we find that the phase current gets limited to 200A peak. When...

PAlva.1 by Associate
  • 2702 Views
  • 4 replies
  • 0 kudos

How to implement speed feedback with B-G431B-ESC1 . I am trying to use this ESC to drive a hoverboard hub motor. Motor profiler works, and I can build an application that lets me run at max speed. Need speed feedb

I am trying to use this ESC to drive a hoverboard hub motor. Motor profiler works, and I can build an application that lets me run at max speed. Need speed feedback to control torque at lower speeds. The motor has both hall sensors and an encoder in...

MCohn.1 by Associate
  • 1400 Views
  • 2 replies
  • 0 kudos

Resolved! Hall Sensor Control w/ STEVAL-SPIN3202

I am using the MC Workbench tool to drive a 3-Phase BLDC Motor with Hall Sensors. I have enabled the hall sensors in the workbench, downloaded the code and flashed my board. How do I actually use the Hall sensor to control the speed? No matter what s...

nmamore by Associate II
  • 3507 Views
  • 6 replies
  • 0 kudos

What is the Hall sensor MTPA?

What is MTPA in the MC workbench speed position feedback management --> Hall sensors? This is NOT the Maximum Torque Per Amp, I believe. Any reference for this?Thanks for reading.

0693W000002liptQAA.png
hmc by Associate III
  • 2286 Views
  • 2 replies
  • 0 kudos

current limit for b-g431b-esc1

Hello,i'm using a b-g431b-esc1 with a 12 V sm-pmsm motor. After running the motor profiler and the motor control workbench, i've played with the cube ide. I have noticed the motor doesn't draw more than 1,6 A, but max current was set to ~5 A in the m...

cz by Associate
  • 1415 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.