2020-08-31 1:15 AM
Hello,
i'm using a b-g431b-esc1 with a 12 V sm-pmsm motor. After running the motor profiler and the motor control workbench, i've played with the cube ide. I have noticed the motor doesn't draw more than 1,6 A, but max current was set to ~5 A in the motor profiler. In pmsm_motor_parameters.h is a define for the nominal current which is set to 1,6 A, but changing it doesn't seem to affect anything. Do you have any ideas how to approach the problem?
Greetings
2020-09-02 5:54 AM
Here some additional context:
2021-06-21 9:50 PM
The question has been moved from the "STM32 Motor Control" section to the "Motor Control Hardware" section (the question is not about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.