STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

To Choice a kit for PMSM

Help me choose a evaluation kit for control PMSM (FOC) with encoder for learning. I need used Motor control Workbench with motor profiler with examples. I need to change code by CubeID and CubeMx and build graphs (STM32CubeMonitor).I want to buy EVAL...

EVALKIT-ROBOT-1 No firmware loaded?

Hello,I have EVALKIT-ROBOT-1. I am working on connecting the device but I couldnt make it.Here are the marks what I did:1) The motor encoder and power cables connected to J12 and J10 respectively on the kit.2) I connected A and B lines between my iso...

OYILD.1 by Associate
  • 1891 Views
  • 5 replies
  • 0 kudos

How to generate motor *.stmcx file from *.xml file

This is a basic question but has me stumped. I have an existing motor project with a *.stmcx file. I generated a new *.xml file for the motor using the profiler. How do I get the *.xml file converted over to a new *.stmcx file? I can load the existin...

BTrem.1 by Senior II
  • 866 Views
  • 1 replies
  • 0 kudos

I like to know why can not read the motor parameters from my evaluation board STEVAL-SPIN3202 using the ST Motor Profiler software and i need to buy an new board B-G431B-ESC1?

My company develop a new BLDC Drive board in order to control a BLDC Motor For use in automatic doors mechanism.i attach the datasheet of the motor. The electrical parameters of motor is the following:1. Number of polar pairs : 22.Max.application spe...

SVlac.1 by Associate
  • 2003 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.