STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Help controlling to stable IQ,ID setpoints, logging values

Newb question here. I have the ST FOC and 6step motor control kit (Nucleo F302R8 , X-Nucleo- IMH07M1 and running bull BR2804-1700KV-1. I have been able to successful using the startup guide for motor control workbench to build and download a configur...

DKASA by Associate II
  • 1969 Views
  • 2 replies
  • 0 kudos

STEVAL-SPIN3201 compilation - FLASH region is overflowed

Hello,I just received the eval board STEVAL-SPIN3201 and am following the document UM2152. Configuration-wise everything seems OK, but I am encountering a compilation problem, the FLASH region is overflowed:>> MOTOR_0001.elf section `.text' will not ...

LCRUZ.9 by Associate II
  • 2293 Views
  • 3 replies
  • 0 kudos

esc001v1 does not connect to motor control workbench

Hi. I'm trying to control bldc using esc001v1, but I cannot connact to motor control workbench.And motor profiler doen't works too.When I using motor profiler, it tells me that f/w doesn't match and after upgrade the f/w, it telling me that serial po...

Rsi by Associate II
  • 2042 Views
  • 5 replies
  • 1 kudos

X-NUCLEO-IHM08M1 peak current higher than 30A ?

What would be the maximum safe peak current for the IHM08M1 board ( 0.5 sec)?I know that the board has a hardware over-current protection kicking in at 30 A. But the STL220N6F7 FETs are rated higher.Also, while configuring the combo X-NUCLEO-IHM08M1 ...

Jay1 by Associate II
  • 1079 Views
  • 1 replies
  • 0 kudos

Motor stops during ramp-up

I could use some help in getting my motor controller through starting the motor. It tries, but always fails to completely start up.I'm working on developing a custom motor control demonstrator board, built with discrete components in the power stage....

0690X000008A7kBQAS.png 0690X000008A7kkQAC.png 0690X000008A7lOQAS.png 0690X000008A7n6QAC.png
RKeny by Associate II
  • 2078 Views
  • 4 replies
  • 0 kudos

When executing the Project Generation command from ST Motor Control Workbench I always get a javax.net.ssl.SSLHandshakeException error showing.

Version info:  MC Workbench      : 5.3.2.18569 WB_to_Mx          : 0.15.6.template-19-01-16 STM32CubeMX       : 5.1.0 MC Firmware Library: 5.3.3Generation options:  Target Toolchain  : ST TrueSTUDIO Target Driver     : HAL - Hardware Abstraction Laye...

Steval Spin3202 - Motor doesn't work ("over-current") ?

Hello,i want to test a BLDC-Motor with the STEVAL-SPIN3202 board. I followed the steps of the datasheet "Using STM32 motor control workbench with STSPIN32F0" to configure the library and generate the code. If i want to start the Motor, I directly get...

TKlei.5 by Associate III
  • 1434 Views
  • 4 replies
  • 1 kudos

MCSDK 5.3.3: code wont execute_ TIM1

Hi,I'm developing an Motor application using F446RE and MCSKD on custom board and custom motor control project, but the program never reaches the user code while loop. I generated the code with ST Motor Control Worbench with 5.2.0 Cube MX andFirmwar...

GBeno by Associate
  • 981 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.