STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

I am getting this warring message "These IPs still have some not configured or wrong parameter values:[ADC1]" when trying to generate code on ST Motor Control Workbench

HI,I'm trying to use ST Motor Control Workbench to make a project for control PMSM Motor,But when i click on generate code.I get this warring message "These IPs still have some not configured or wrong parameter values:[ADC1] Do you still want to gen...

Mr.SU by Associate II
  • 1948 Views
  • 5 replies
  • 0 kudos

Steval-spin3201 hall sensors connection.

Hello!I'm trying to work with steval-spin3201 board, i have AMETEC minijammer bldc motor with three hall sensors on board, ST Motor Control Workbench with Atolic True studio. First i tried sensor-less control and it's works fine with some tuning. But...

Roman by Associate II
  • 1770 Views
  • 3 replies
  • 0 kudos

MCSDK-5.4.0 to CubeIDE problem

Using "Motor Control Workbench" I created a project for the following hardware:NUCLEO-F303RE + X-NUCLEO-IHM16M1.I did not make any changes to the standard configuration.I generated the files by setting the TARGET to CubeIDE with firmware package FW V...

MCSKD 5.4.0 HardFault

I did some tests using the MCSDK 5.4.0, I generated the project using MC WorkBench for TrueStudio and CubeMX 5.2.1.The hardware consists of NUCLEO-F303RE and X-NUCLEO-IHM16M1.The problem is the following: when I try to start the engine with WorkBench...

0690X000008ichgQAA.jpg 0690X000008iciFQAQ.jpg 0690X000008icioQAA.jpg

Using STM32F103VC in MC workbench

Hi, I have some question on mcu selection in MC workbench. As I have previous build an application based on STM32F103VC, I would like to use MC workbench to do configration. However, i cannot select it from the list. Are there any other solution? Tha...

Ysiu by Associate II
  • 1199 Views
  • 2 replies
  • 0 kudos

Drive 48V Conveyor Drum Motor using STEVAL-SPIN3201

Hello Community,I have purchased a STEVAL-SPIN3201 eval board last week. I want to drive a 48V Drum motor using this eval board with Motor Control Workbench 5.40. But I don't have the full motor parameters. Based on the user manual UM2152, the motor...

0690X000009YKdRQAW.jpg
LXian.0 by Associate II
  • 1970 Views
  • 3 replies
  • 0 kudos

Motor control Workbench is generating code with errors

i am using STEVAL-SPIN3201 development board for the project.first i start the workbench and give the board details then after setting i give to generate code.the workbench is giving the code with errors.why this happens...?i am attaching my log whic...

NK.13 by Associate II
  • 983 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.