2019-04-10 7:41 AM
Version info:
MC Workbench : 5.3.2.18569
WB_to_Mx : 0.15.6.template-19-01-16
STM32CubeMX : 5.1.0
MC Firmware Library: 5.3.3
Generation options:
Target Toolchain : ST TrueSTUDIO
Target Driver : HAL - Hardware Abstraction Layer
Target STM32 FW : 1.9.0
Updated ioc: C:\xxxx\xxxx\xxxx\xxxx\xxxx\xxxx\xxxx.ioc
Generating...
C:\xxxx\xxxx\xxxx\xxxx\xxxx\xxxx\
...\.extSettings
Code generation started
Exception in Publisher javax.net.ssl.SSLHandshakeException: Remote host closed connection during handshake
...\Src\motorcontrol.c
...\Inc\motorcontrol.h
...\Inc\drive_parameters.h
...\Inc\mc_tasks.h
...\Src\mc_api.c
...\Src\motor_control_protocol.c
...\Inc\mc_api.h
...\Src\mc_config.c
...\Inc\mc_config.h
...\Inc\mc_stm_types.h
...\Src\mc_tasks.c
...\Src\regular_conversion_manager.c
...\Inc\regular_conversion_manager.h
...\Inc\parameters_conversion.h
...\Inc\parameters_conversion_f0xx.h
...\Inc\pmsm_motor_parameters.h
...\Inc\power_stage_parameters.h
...\Src\stm32f0xx_mc_it.c
...\Inc\mc_parameters.h
...\Src\mc_parameters.c
...\Src\ui_task.c
...\Inc\ui_task.h
...\Src\user_interface.c
...\Inc\user_interface.h
...\Src\stm32f0xx_it.c
...\Inc\stm32f0xx_it.h
...\Src\stm32f0xx_hal_msp.c
...\Inc\stm32f0xx_hal_conf.h
...\Inc\main.h
...\Src\main.c
Completed with errors
2019-04-11 7:26 AM
Same for me, but it appears quite "randomly".
The very next compile-attempt almost always works without me changing a single thing though.
2019-05-11 1:17 AM
After upgrading MX , I met similar problems.
Anyway I solved the tartet STM32 setting by "latest"
Target STM32 FW : Latest
2021-06-22 1:44 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.