2019-03-27 7:19 AM
What would be the maximum safe peak current for the IHM08M1 board ( 0.5 sec)?
I know that the board has a hardware over-current protection kicking in at 30 A. But the STL220N6F7 FETs are rated higher.
Also, while configuring the combo X-NUCLEO-IHM08M1 with a NUCLEO-F302/303 in motor control workbench, you can optionally use comparators on the MCU board for the over-current protection. With the MCU comparators OCP is configurable to kick in as high as 99 A.
Is the X-NUCLEO-IHM08M1 capable of handling 99 A(peak) for let's say 0.5 second?
If not, what would be a safe peak current (and duration) to be handled by the X-NUCLEO-IHM08M1?
Thanks in advance.
Jay
2021-06-22 1:47 AM
"STM32 Motor Control" topic added.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.