2019-04-13 7:00 AM
For our project we want to know the motor parameters of a custom 1.4KW (2HP)Motor. Photo attached.
we are using Motor profiler on STM3240G-Eval with STEVAL-IHM028V2.
The problem is The profiler is failing in its initials stages and not able to identify Rs and Ls.
Its Shows 0 RPM and after some time shows a massage "The measurement is talking two much time"
We have taken care to properly configure boards in motor Control Mode.
your suggestions Please...
2021-06-27 9:52 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.