2020-04-08 3:41 AM
I stay try to run this example on my board in PIL mode(i change project target to stm32.tlc instead the buildin stm32f302r_nucleo) , but i receive from sw4stm32 error for missing arm_math.h . I include the link to the file from the stm32cube repository, and after i have FPU error. when in the preprocessor i add " __FPU_PRESENT " the error go to arm_cos_f32....
How i can solve it? How i must setting the parameters in simulink or eclipse?:face_with_steam_from_nose:
2021-06-28 3:28 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.