2015-03-25 5:38 AM
Hi,
I like to test the HFI function on the STEVAL-IHM042V1. Without HFI is the motor running well. But how can I implemented the HFI? I followed the instruction of UM1052 page 65. But I can not configure the DAC in the STMCWB. Because DAC1 is used for the OCP and DAC2-pin is input for the MC1currentA. What's the best way to do this? Thanks,2021-06-28 3:25 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.