STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Why does the CCR value not Updated?

Hi All,I would appreciate your help with this problem.I am presently trying to implement the PWM scheme PWMON as shown in figure below.I have set the polarity of the timer's main and complementary output to be LOW. And it runs on PWM Mode1.And then a...

0693W000008xZwfQAE.png 0693W00000BajEyQAJ.png 0693W00000BajJsQAJ.png

Speed Control of 3-Phase Induction Motor

I'm designing project for Speed Control of 3-Phase Induction Motor with STGIPS30C60-H. I'm driving with microcontroler trough optocoupler. The motor is rotating in with desired speed about one minute and after stop. After that STGIPS30C60-H does not ...

MTole by Associate II
  • 1370 Views
  • 1 replies
  • 1 kudos

Resolved! AC Servo motor solution

Hi all,Does ST have any solution for Development of Driver circuit of "Permanent magnet synchronous AC servo motor" and "AC induction servo motor".

sanju by Senior
  • 1492 Views
  • 2 replies
  • 0 kudos

Resolved! Do X-CUBE-MCSDK will support AC induction motors?

Posted on June 17, 2018 at 12:25Hello,For the moment, X-CUBE-MCSDK only support PMSMs and BLDC motors.However, AC inductions motors are not supported yet, that's a shame because this kind of motor is still very present in the majority of industrial ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.