STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

I am using MCSDK5.Y.2's electric output library. How can I change the current parameters of the motor by directly modifying the source code?

我用的是MCSDK5.Y.2的电出库,�?如何通过直接修改�?代�?,改�?�电机的电�?�?�数?(�?用�?新�?用STM32Cube�?次生�?)我修改了M1_ApplicationConfig_reg.maxMotorCurrent的值,但是�?�有界�?�显示�?�化,实际电�?并没有�?�化。我修改了M1_MotorConfig_reg.maxCurrent值,什么没有�?�化。

ZXuey.1 by Associate II
  • 1125 Views
  • 1 replies
  • 0 kudos

How to start with 3-Phase BLDC motor:

Hi,I have to make low cost on BLDC for Industrial Sewing Machine with Three Hall Sensors and read about BLDC from resources available on internet . I have P-NUCLEO-IHM001 for BLDC motor controland seen below youtube video from ST.https://www.youtube....

Are there STM32 based PLCs out there?

I'm looking at different alternatives for PLCs and I would love to use STM32 as one, but it seems like the boards that STM sells are all eval boards or individual boards. I'm lookin for a completed product that has stepper motor control and GPIO. I...

msche.1 by Associate III
  • 1607 Views
  • 2 replies
  • 0 kudos

How to successfully debug a ST FOC motor control project ?

I'm working on a project where the STMC FOC v4.3 SDK has been used. Developers of the project are not available for support, and I need to learn the details to implement new features as well as debugging/fixing existing code.To facilitate my learning...

c1ron by Associate III
  • 2790 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.