2022-01-26 2:27 AM
Is there an assumption that the motor parameters are for a star connected motor when setting them in the STMC Workbench ?
If your motor is delta-connected, then can you put values given in the motor datasheet directly (winding resistance Rs, inductance Ls and back-emf constant, etc) or do you need to convert them according to the figure ?
Solved! Go to Solution.
2022-01-26 5:12 AM
> Is there an assumption that the motor parameters are for a star connected motor when setting them in the STMC Workbench ?
No there are not.
If you consider your motor as a black box, Rs is the resistance measured between two phases divided by 2, and same thing for Ls.
More information can be find here.
Regards
Cedric
2022-01-26 5:12 AM
> Is there an assumption that the motor parameters are for a star connected motor when setting them in the STMC Workbench ?
No there are not.
If you consider your motor as a black box, Rs is the resistance measured between two phases divided by 2, and same thing for Ls.
More information can be find here.
Regards
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.