2021-12-22 9:52 PM
2022-01-10 5:06 AM
Hello @AFirt.1 and welcome to the ST Community.
As reported in the EVALSTDRIVE101 user manual UM2781 the J2 jumper allows to short the DT/MODE pin of the STDRIVE101 to GND, thus enabling the INH/INL mode.
If left open, the STDRIVE101 is configured in EN/IN mode.
When the STDRIVE101 is configured with ENx/INx input strategy, the half-bridge “x�? is enabled or disabled by ENx signal and its status is determined by INx signal.
Morevoer, the deadtime is set by R6; the default 51 kΩ resistor gives a deadtime approximately around 570 ns.
You can find more details about the control logic in the STDRIVE101 datasheet (page 17 and following).
Let me know if I fully answered your question, if so please "Select as Best" label.
2022-01-24 7:18 AM
Hi @AFirt.1 any feedback? Have I solved your doubts?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.