STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

When PWM duty changes?

Hello,I control BLDC motor.Control the speed of the motor by changing the TIM->CCR.​I have a question while setting the time to change the value of CCR.If I change the value of CCR while I'm sending out PWM, will the Duty ratio change in the next cyc...

hjuns by Associate III
  • 1269 Views
  • 1 replies
  • 0 kudos

Resolved! [Bug report MCDSK 6.0.0] Missing files when generating code with "Copy only the necessary files" option

The MC Workbench tool generate a CubeMX 6.5.0 project, that in turns generate C code.Actual behaviorWhen I select in this CubeMX project Project Manager > Code Generator > Copy only the necessary files, the generated IAR 8.0 project does not compile ...

My ST-Link/V2-1 doesn't work after upgrading FW

Hi!My ST-Link/V2-1 of NUCLEO-F302R8 doesn't work after upgrading ST-Link/V2-1's FW to latest version. Using lsusb it seems appear: Bus 001 Device 008: ID 0483:374b STMicroelectronics ST-LINK/V2.1However, STLinkUpgrader says something wrong with it...

0693W00000Uo8XSQAZ.png
OChen.1 by Associate II
  • 1441 Views
  • 1 replies
  • 0 kudos

MC SDK long response time after wakeup from stop mode

I'm working on a project whith use a STM32F407 MCU to control a bldc motor and also has a low power mode, the mcu will into stop mode.Now the stop mode is working, and we have issue to control the motor after wake up from stop mode.​the code to enter...

0693W00000UoEHQQA3.jpg
Guopeng by Associate II
  • 1104 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.