STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4991 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! not enough torque

Good morning , I'm writing this post to request help , the main problem is two things the first and the main thing being the 1000W 3500 RPM 3 pole pair 48V motor not giving it rated torque of 2.5 Nm and only gives 0.8 N.m , this was confirmed as the ...

Nontinium by Associate II
  • 1319 Views
  • 6 replies
  • 0 kudos

Resolved! STEVAL ESC001V1 PID Tuning

When i give varying PWM signal at high frequency under range, the motor sometimes produces noise and gets stuck (0 speed even though pwm signal is valid). What is the issue? I feel its due to PID tuning. Kindly share PID tuning method.Thanks 

Resolved! FOC Control with STM32G491KE

Hi, I'm a circuit engineer in korea.I want to make really small BLDC FOC controller with STM32G491KE, because It has the smallest pin counts compare to other G491 family.For FOC Control, I have to use three TIM channel. For use external ociliator, I ...

yeseung_0-1767350262868.png
yeseung by Associate
  • 1006 Views
  • 4 replies
  • 0 kudos

How to add inverter board in MCSDK6?

Hi there,My team has designed a dual motor control board, and I'm responsible for spinning the motors.I have already added the board to MCSDK6 and generated the project without error.However, when I add the code like MC_StartMotor1() after initializa...

Junde by Senior III
  • 430 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.