STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! MCWB 6.1.2 Doesn't allow hall sensor + QuadEnc

The MCWB 6.1.2 doesn't allow the configuration of of both hall sensor and quadrature encoder as speed/position sensors in main/auxiliary speed sensor configurations. It looks like the only conflict is in timer input pin allocation, but it seems like ...

Resolved! Power factor correction in MCSDK

I have seen the Digital PFC section in MCSDK 6.1.2 but i do not get an option in the project i have selected for the B-G431B-ESC1 project. How can i enable it? How important is this Digital PFC? In my testing i get around 0.6. 

SRedd.5 by Senior III
  • 1263 Views
  • 1 replies
  • 0 kudos

Resolved! How to configure 3 Shunt 3 ADC measurement

Hi,I have a STM32G491 based design with three differential shunts, routed to the three Op Amps of the MCU. I would prefer to run the Op Amps in standalone mode. This would allow me to have a low pass filter (cap across negative and output) and I woul...

JKolj.1 by Associate III
  • 3966 Views
  • 3 replies
  • 2 kudos

Resolved! Using MCSDK / Motor Pilot in a virtual machine

Unfortunately MCSDK is not available for Linux. So I have installed it on a virtual machine. But the application "Motor Pilot" doesn't work. It even doesn't start.I have tried with MCSDK 6.1.1 and 6.1.0, with Windows 11 and Windows 7, withOracle VM V...

Marc1 by Associate III
  • 2149 Views
  • 1 replies
  • 0 kudos

Resolved! Systick time missing

I am running the motor control workbench B-G431B-ESC1 board. The systick fires at every 2K frequency as per the user manual and the waveform matches when i toggle, but the problem is sometimes it misses as shownI want to debug and find out why it mis...

SRedd5_0-1689998582490.png
SRedd.5 by Senior III
  • 12375 Views
  • 23 replies
  • 1 kudos

Which power board should I choose?

Hi,I want to control a PMSM using STM32 FOC SDK.And the spec of the PMSM is belowRated input volt: 62 VRated current: 2.5 ARated output: 200WBut I notice the voltage sets of power broad are10~28 Vdc8~48 Vdc125~400 Vdccould I choose 8~48 Vdc range to ...

Erem by Associate
  • 1528 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.