2022-04-26 10:05 AM
Hi,
I want to control a PMSM using STM32 FOC SDK.
And the spec of the PMSM is below
Rated input volt: 62 V
Rated current: 2.5 A
Rated output: 200W
But I notice the voltage sets of power broad are
10~28 Vdc
8~48 Vdc
125~400 Vdc
could I choose 8~48 Vdc range to control my PMSM?
Like X-NUCLEO-IHM08M1 power board.
(But the motor speed may slower than the value on datasheet)
Or should I follow the Watt?
Like STEVAL-IPM05F (500W power board).
(But I am not sure the output voltage will under 62V or not)
2023-09-22 1:38 AM
Hello @Erem
I suggest the St Mc Suite tool, which lists you the Motor Control compatible boards with the details, Here is the link : https://www.st.com/st-mc-suite/home/
We are sorry for the late response, if you still need help,
- Click on - Start -> Engine Control Solution
- select the motor type (BLDC)
- select the algorithm
- then choose your board in Power Board
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.