STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! EVAL6498L High side problem

Hi Everybody!At this time I would like to use two EVAL6498L board for a DC brushed motor, (H-bridge setup).Selected mosfet is: IRFZ34NPBF.Selected PWM frequency: 20kHz width the STM32G431 MCU.The PWM signals are generated on the GPIOs, and I’ve verif...

ProgBoy by Associate
  • 785 Views
  • 1 replies
  • 0 kudos

Resolved! steval_esc001v1 help

my mcsdk ver is 6.3.2,I want to driver my BLDC moto with steval_esc001v1,but the moto will stop and shake after 3-phases speed up. as the motor shake,and bus voltage(current) shakes.i want to know the Possible causes and how shuld to solve it.my moto...

shanjie by Associate
  • 873 Views
  • 5 replies
  • 0 kudos

Resolved! STDRIVE102P - 'P' variant?

What is the P variant of STDRIVE102 and how does it vary from the STDRIVE102H?I can find datasheets for STDRIVE102H/STDRIVE102BH - with the BH variant having 3 Shunts(OpAmps) vs the standard H having 1 Shunt(OpAmp).The boards manager in ST Motor Cont...

CraigP by Associate
  • 731 Views
  • 2 replies
  • 1 kudos

Resolved! X-NUCLEO-IHM16M1 Max Current

I am currently using the X‑NUCLEO‑IHM16M1 expansion board and noticed a discrepancy between the Motor Control Workbench and the official ST documentation regarding the rated current.In Motor Control Workbench, the Rated Current is shown as 2.1 A.On t...

pelino by Associate III
  • 910 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.