2024-08-20 7:28 PM
Dear All,
I just stat to evaluate the MC SDK.
My platform: MC SDK v6.3.0, NUCLEO-H563ZI, X-NUCLEO-IHM08M1.
Have anyone know what's the difference between "Dead Time" and "SW Dead Time" as follow figure?
Per it's default configuration, (SW dead-time is 850ns, dead time is 1000ns), what is the exact value of dead-time to the power stage?
Best Regards,
2024-08-26 3:58 AM
Hi All,
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Jake
ST Support
2024-08-29 12:57 AM
Since this is a community forum and others (me included) might be interested in the solution to this question as well, could you put the answere here?
2025-08-26 8:49 AM
2025-08-27 7:05 AM - edited 2025-08-27 7:05 AM
Hello @OHarc.1 ,
Thanks for your interest on this topic!
I am checking with our Online support team if they can provide a public response to this. Thank you for your patience.
Regards,
Lina
2026-01-15 12:42 AM
Hello @Lina_DABASINSKAITE
Do you have any update on this? I am also curious what the answer is.
2026-01-15 2:39 AM
Hello @bingbong,
Refer to the PWM generation chapter in the MCSDK6.4x user manual, which is available through "Workbench tool > About > Documentations > Documentation".
2026-01-15 3:09 AM
Thanks!
For anyone wondering, it is in this path:
*MCSDK_INSTALLATION_PATH*\Documentation\html\md_docs_2_p_w_m___generation.html
In my case, this was: C:\Program Files (x86)\STMicroelectronics\MC_SDK_6.4.1\Documentation\html\md_docs_2_p_w_m___generation.html
Anyways, the short version is that "dead-time" is a fixed hardware value used only for calculations when driving high sides and enables. This is defined in the board .json file as "deadTime". The "SW dead-time" is a configurable value actively written to the timer register when driving both high and low sides. The range available is defined by "minDeadTime" and "deadTime" in the board .json file.
2026-01-16 2:06 AM
Hi @bingbong,
Please see the latest reply by @GMA : Re: What is the difference between "Dead Time" and... - STMicroelectronics Community.
Regards,
Lina
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.