STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

MCSDK 5.y serial communication RS-485?

Hi,My custom board has an STM32G474RE with an RS-485 port that I would like to use to communicate with the Motor Pilot software. Is it possible? I tried to use the STM32CubeMX to activate the UART5 hardware flow control (DE) but the connection failed...

Asantos by Senior
  • 2223 Views
  • 4 replies
  • 0 kudos

EVSPIN32F0602S1

Hi,In the generation, warning and fatal errors are occurred as attached,What's the reasons of these faults and,How I can solve it ? Evaluation Board : EVSPIN32F0602S1.MotorControl Workbench V5.4.8STM32CubeMX5.6

화면 캡처 2023-11-23 134809.png
yourbryan by Associate II
  • 2301 Views
  • 3 replies
  • 0 kudos

Help creating a circuit

How to create a microprocessor system that can drive a stepper motor, where the motor, not being a component of the microprocessor system, is externally powered via a diode to meet its voltage requirement exceeding 3.3 V?

dual encoders

Hello everyone I am looking for some support with using 2 encoders on an STM32F303CB. I am able to select in the Motor Control workbench to have an encoder on Tim3 (pins B4 and B5) or on Tim2 (pins A5 and B3). I need to use 2 encoders for a project. ...

Resolved! STOPPING PMSM MOTOR

Hi,We are using MCSDK_v5.Y.4. We would like to implement Stall Detection and are considering using the measured iq current (used in FOC) for detecting a motor stall. We intend to use a Stall_Detection_Threshold, which is just below the "Current_Limit...

jocelync by Associate II
  • 3123 Views
  • 3 replies
  • 1 kudos

Resolved! Stop command and startup with Hall sensors

[VERSION]: MCSDK 6.1.2 and 6.2.0.[TOOL]: MC Workbench, MC Pilot, MC Firmware.[DETAILS]:I developed a control/power board, a custom Hall sensors board and a motor (which will interface a reduction drive) for AGV application. I was able to integrate ve...

pzt by Associate III
  • 6376 Views
  • 3 replies
  • 0 kudos

warum dreht sich mein Motor nicht

ich verwende MCSDK 6.2.0 ich versuche seit einigen Tagen ein Maxon-Motor mit B-G431B-ESC1 zu drehen. aber es gelingt bisher nicht. Könnte jemand mir bitte sagen , was ist falsch eingestellt habe? ich habe mit Workbench alle Parameter von meinem Motor...

Jess32 by Associate II
  • 2390 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.