STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Using MCSDK API

Hardware:B_G473E_ZEST1S - Control boardSTEVAL-LVLP01 - Power boardMOONS R57BLB50L2 BLDC motorSoftware:MCSDK 6.2.1Code framework generated by MotorControl Workbench v6.2.1IDE STM32CubeIDECode customized only in main.c.  See attached.I was able to get ...

ccut93 by Associate III
  • 4700 Views
  • 2 replies
  • 0 kudos

Motor Control Workbench

Hello guys, I want to control an AC servo motor (ELM2H-0400LA60F) and a Motor Driver (RS-400P) with an STM32f407 discovery kit. But I cannot find my motor and control in the MC Workbench. Is it possible to work with MC Workbench in this regard?? 

STM32F407 Using GPIO to generate 5V PWM

I am working on the STM32F407 and we made some bad choises when selecting a motor. The motor control signal is 5V hence we need to generate 5V PWM signal using the STM32F407. Sadly, we have wired the GPIO from the STM32F407 directly to the motor cont...

LPetr1_0-1707223802637.png LPetr1_0-1707224113013.png LPetr1_0-1707225389413.png LPetr1_1-1707225618823.png
LPetr.1 by Senior II
  • 6200 Views
  • 4 replies
  • 7 kudos

Resolved! Cannot Launch a MC Workbench project with STM32G431CBUx mcu

I am trying to launch a MC Workbench project targeting a STM32G431CBUx mcu as the controller. I tried to modify an existing control board file to use the STM32G431CBUx as the mcu. I am able to select my custom control board on the selection page, as ...

captat by Associate II
  • 2063 Views
  • 1 replies
  • 1 kudos

How to profile a motor with Rs<1Ohm, Ls<1mH ?

According to here:https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:Frequently_Asked_Questions#Why_does_not_my_motor_start_immediately-3F The STM32 MC motor profiler has the following limitation: it cannot profile motors with Rs < 1 Ω or Ls < 1 mH....

SKled.1 by Senior II
  • 3538 Views
  • 4 replies
  • 0 kudos

STSPIN32F0A configure PWM input

Hello,is there is an option of adding input pin for external PWM? I want it for ESC, I would like to control it with PWM signal like on board B-G431B-ESC1. I tried with STSPIN32F0A board example, however adding ESC to .json file doesn't do anything. ...

esc.png

Resolved! Flux Weakening

Hi Team,I have enabled the flux weakening for the Motor. But as per my understanding, flux weakening helps us to run the motor beyond the rated RPM. But in my case, I am not able to see that difference.Could you please help me understand how it works...

Akhilesh30_0-1707129902511.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.