2024-02-04 2:31 AM
Hello,
is there is an option of adding input pin for external PWM? I want it for ESC, I would like to control it with PWM signal like on board B-G431B-ESC1. I tried with STSPIN32F0A board example, however adding ESC to .json file doesn't do anything. I added with PA6 pin from STEVAL-ESC002V1 schematic. The attached photo is for B-G431B-ESC1 and I would like to enable it also for STSPIN32F0A. Could you please tell how to configure the board for PWM input? Thank you!
Kind regards,
JS
2024-02-05 5:56 AM
Hello @JosefSchon ,
Unfortunately, not yet.
This feature is more applicative than a part of the library itself. We developed it to satisfy the requirement of our B-G431B-ESC1 board but we did not generalize it yet to all the families.
Nevertheless, nothing is preventing you to generate the B-G431B-ESC1 example and do the porting to your STSPIN32F0A board.
The generalization of this feature is planned for this coming year.
Regards
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.