STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

B-G431B-ESC1 / - Speed error

Hello. I'm using B-G431B-ESC1 to operate drone motorThe operation was successful using FOC, but from 28,000 RPM and above,it changes to - speed as seen on the Pilot screen. (When the rpm becomes negative, speed control becomes impossible.)In fact, us...

LeeYoung_0-1769071420130.png
LeeYoung by Associate
  • 378 Views
  • 3 replies
  • 0 kudos

ST SPIN MTPA slope and offset array

Can anyone help me understand how these two arrays have been made#define M1_ANGC                            {-116,-363,-611,-843,-1091,-1338,-1571,-1833}#define OFST {0,17,51,99,167,252,348,474}these arrays are used in MTPA calculation with y=mx+c eq...

RAlph1_0-1768390301357.png
RAlph.1 by Associate
  • 234 Views
  • 1 replies
  • 0 kudos

Parameter configuration for High Speed BLDC Motor

Hello,I am below Hardware and Software setup:Hardware:MCU Board: NUCLEO F401REPower Board: X-NUCLEO IHM08M1BLDC Motor: Portescap 22ECP45-8B-154.01 (specifications_22ecp45.pdf attached)Software:MC Workbenach v6.4.1I am using sensorless FOC (STO-PLL) i...

omkar62_1-1768976587315.png omkar62_2-1768976624497.png omkar62_4-1768976686538.png omkar62_5-1768976717573.png
omkar62 by Associate II
  • 441 Views
  • 2 replies
  • 0 kudos

Resolved! JSON file for a new motor to upload in Workbench?

Hello. I try to start a new project with two non-listed motors in Workbench. I use two gimbal 3-phase BLDC motor with encoder AS5048A https://cdn.sparkfun.com/assets/d/6/b/5/8/27477_27478_Datasheet.pdf Based on the motorShinano.json file, I built my ...

Boris_L by Associate II
  • 787 Views
  • 3 replies
  • 0 kudos

BLDC motor calculate peak phase current

Hi,How can one calculate the maximum phase current of a BLDC motor using sinusoidal control with the nominal voltage and power of the motor?I have a 36 V / 560 W motor.Is the peak current equal to:560 W / 36 V * SQR(2) =  22 Aor beacuse of the star t...

rogdiv by Associate II
  • 236 Views
  • 0 replies
  • 0 kudos

STEVAL-ESC002V1 with NUCLEO-F031K6 board

Hello. I have been researching how to use the STEVAL-ESC002V1 with a NUCLEO-F031K6 board to run a BLDC motor. The documentation mentions using the IAR Embedded Workbench for ARM 8.22, but I am programming with the STMCubeIDE and the MotorControl Work...

gndLD by Associate II
  • 562 Views
  • 5 replies
  • 1 kudos

Low speed control algorithms with sensors

Hi - What is the best algorithm for a very low speed and low current application, <50 RPM and <1 Amp with a high resolution encoder (~4096 counts per revolution) on a 3 phase brushless motor? Do the HSO or ZEST algorithms provide any advantage over t...

geneM by Associate II
  • 777 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.