2026-01-23 12:36 AM
Hi,
How can one calculate the maximum phase current of a BLDC motor using sinusoidal control with the nominal voltage and power of the motor?
I have a 36 V / 560 W motor.
Is the peak current equal to:
560 W / 36 V * SQR(2) = 22 A
or beacuse of the star topology of the motor:
560 W / 36 V / SQR(3) * SQR(2) = 16.33 A
I need this to select the proper FETs.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.