STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

I couldn't drive bldc motor with the Steval-spn3202

Hi all;I use the Steval-spn3202 control driver and x-cube-mcsdkh 5.6.0. I use the parameter of bldc motor is 12W, 12000rpm, 0.2A(Nominal current), 24V, 8ohm, 0.488H, 1.95 V/krpm.I want to control speed control or torque control with foc so that first...

mkk.1 by Associate II
  • 4100 Views
  • 7 replies
  • 0 kudos

HALL sensor Pin out only 3.3v

Hello guys I'm trying to do a profiler for Hall sensors.But when I measured my Hall power pins they only provide 3.3V instead of 5.0V and my Hall sensor needs at least 4.5V, I tried to check my control board manual and found that my SW is in the righ...

poyilee by Associate II
  • 6716 Views
  • 4 replies
  • 0 kudos

EVSPIN32G4 ADC not working

Hi, Good Morning            I want to control the motor through an analog input (PA4) (ADC2_IN17). However, I am unable to read the ADC value. The generated code lacks the initial configuration for ADC2 channel 17 in the MX_ADC2_Init() function.Pleas...

EVSPIN32G4 FOC_SPEED MODE

I am planning to drive the motor with FOC using the EVSPIN32G4 board.MC_WorkBench 6.3.0ST Motor Pilot V1.2.0 - profilerI checked the motor parameters with the ST Motor Pilot V1.2.0 - profiler program.And I created a project with the EVSPIN32G4 board ...

Sensorless FOC and high electrical frequency

Dear MCSDK,Thnak you for your nice work with this project. I am trying to use the McSDK with ST eval board B-g431-sec to control the speed of a small brushless PMSM motor with sensorless FOC.This motor with its load can rotate at approximately ~10k r...

ANICO.1 by Associate III
  • 4543 Views
  • 6 replies
  • 0 kudos

How to clear FAULT NOW startup error

When I try to start my motor by programming a torque ramp and starting the motor, if the motor fails to start, the motor state moves to FAULT_NOW with a startup error. The real issue is that I don’t know how to clear the fault. The state never change...

captat by Associate II
  • 3947 Views
  • 3 replies
  • 0 kudos

Resolved! MC Workbench 6.3.0 - Generation of project fails.

Hello there,I am new to the MC Workbench and must configure the B-G431B-ESC1 to use it with a A2212/6T 2200KV Brushless DC Motor.I created a new project in the MC Workbench 6.3.0 and tried generating the project. Once the generation is completed I re...

STMBatu_0-1715772920498.png
STMBatu by Associate II
  • 5042 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.