STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! EVSPIN32G4 - Frequent Overcurrents

Hi.I'm driving a PMSM with FOC (Workbench file attached for reference) with MCSDK 6.3.0 in torque mode.Main parameters:1400 Hz electrical frequency max -- therefore 16 kHz PWM100 Hz mechanical frequency max~0.03 mH line-to-line inductance~9 V/Hz Kv 0...

grisharevzin_0-1723900399238.png

ST motor pilot V1.2.9 localisation issue

The GUI MC_FOC_SDK is supposed to be able to tune revup parameters. However, if we try to modify variables in the Torque-column (and only in this column), all input is reset to zero:I have tracked the issue down to RevUpComponent.qml -> doublespinbox...

LLang_1-1725367773199.png
LLang by Associate
  • 1263 Views
  • 1 replies
  • 3 kudos

Resolved! Lecture registre HALL_EL_ANGLE ou HALL_SPEED

Bonjour,    J'ai configurer le contrôle moteur avec un capteur effet hall en auxiliaire.le moteur tourne mais les valeur des registre ne change pas. elle prennent une valeur différente a chaque démarrage mais ensuite ne change jamais. Comment vérifie...

Christophe65_1-1724751831609.png

Engine stops after a few seconds.

Hello everyone.I am using the Motor Control WorkBench 6.3.0 application to generate the project. The inverter board isB-G431B-ESC1. The motor is a 2-pole BLDC, 8.5V, it has a very low inductance of 0.04mH, an Rs of 0.37ohms and the B-Emf constant is ...

OttoBCN by Associate II
  • 3783 Views
  • 8 replies
  • 0 kudos

Reset issue STSPIN32F0A

Hello,I have some troubles with the STSPIN32F0A when the load on the motor increases,the STSPIN will reset. The reset cause is checked in firmware at startup, and the cause mentioned is RCC_FLAG_PINRST.Apart from a pull-up and a capacitor to ground, ...

CCarl by Associate II
  • 2453 Views
  • 5 replies
  • 0 kudos

ADC2 configuration issue (injection and regular)

Hi,The version of mcsdk I'm using is 6.3.0, I have a problem with my ADC2, enabling one injection channel as a sample of phase current, and three regular channels, one of which is used as a speedpotentiometer, and two for my own use, and currently ru...

iskan by Associate III
  • 881 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.