STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! evspin32f0602s1 Motor driving C code

Hello, I am very new for ST mc. I want to use evspin32f0602s1 for BLDC motor,I have generated the code using Workbench,STCubemx and finally code seen in IDE,but I dident getting what to write in main() function ,how it can handle any fault situation ...

KVijay32 by Associate II
  • 1518 Views
  • 2 replies
  • 0 kudos

Hardware Flow Control in CubeMx selection

How to enable Hardware Flow Control in STM32 Cube MX , because when I am trying to enable it - conflict with ADC1:IN6 . I want to enable Hardware flow control RS485. I have attached the screenshot of the issue being faced. This program is generated ...

Screenshot (96).png
hu88 by Associate II
  • 1354 Views
  • 1 replies
  • 0 kudos

Resolved! MC 6.3 with MX6.12 - attr not supported : Dmpu

I am trying to generate code for "STM32 Nucleo packs FOC and 6-step motor control platform for three-phase, low-voltage and low-current motor" and I keep getting errors :-Attr not supported : Dmpu  as in attached image. I am using cubeMX12, I have up...

mc.JPG
Sujoy_B by Associate II
  • 17645 Views
  • 18 replies
  • 4 kudos

Resolved! MC Workbench Phase Voltage Sensing

Hello,I am designing FOC motor controller based on DRV8316. For this, I am adding a DRV8316 custom board in the MC Workbench. Please find the JSON file attached. The problem is that I am unable to add phase voltage sensing. Although I have added phas...

farzansaleem_0-1724785407643.png farzansaleem_1-1724785424396.png farzansaleem_2-1724785589618.png

how to implement ENCODER MoDE using GPIO ?

In my design , MCU controll 8 sets of  STEP MOTOR  .    Every MOTOR  has  A / B Encode pulse outputsIN CubeMx  Six timers (TIM1-TIM5  & TIM8  )can be configured to ENCODER MODE 。  But  How to implement the other 2 Motors decoder ?   Can we use gpios ...

JohnGe by Associate
  • 1065 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.