2026-02-12 10:44 PM
I am using the B-G431B-ESC1 board, which connects to my laptop via a micro-USB to USB-A cable. After a failed connection attempt, the board is no longer detected by STM32CubeProgrammer. Additionally, a file named "File.txt" is created on the MCU after the failed attempt.
The contents of the file are:
"The interface firmware FAILED to reset/halt the target MCU."
This file appears to be causing issues with the connection to STM32CubeProgrammer.
Could anyone please help me resolve this issue?
2026-02-18 2:57 AM
Answer:
In STM32CubeProgrammer, select “Connect Under Reset”
Fully power cycle the board and try again - done during test
Also updated ST-LINK firmware updates
But same result occurs again.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.